Part Number: ISO7741
Other Parts Discussed in Thread: ISO6441
We discovered that the ISO7741FDW is susuceptable to radiated fileds at 1.2GHz and 2.4GHz. A signficant amount of effort was put into tightening the shielding of the electronics encloser and filtering all I/O, but we have not been able to reliably solve the issue. We replaced the isolator with the equivilent Skyworks isolator and have had reliably passing results with no upsets. We would like to know if there are known susceptabilies with the ISO7741FDW. My best guess is that the carrier used for signal transmission must be close to 1.2GHz, and the threat is jamming the transmitted signal. There is an advertised new replacement part on TI's web site, the ISO6441. This is advertised as "EMI robust". Would this part have a better chance of passing radiated susceptability testing?