This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN6507: Information

Part Number: SN6507

Hi Team,

Could you let me know the max. allowed load current.

and could you share me any application note which provides both positive and negative outputs.

Do you have any worst case calculations for this IC  ?

 

Thank you,

Teajsri.

  • Hi Tejasri,

    Please find below input:

    1. Max allowed load current is 500mA.

    2. We have SN6507DGQEVM EVM board which is configured to provide both positive and negative outputs. You can refer to its user guide. 

    i. Link to EVM product folder :- ://www.ti.com/tool/SN6507DGQEVM

    3. You can use Webench Power design tool for calculations - https://webench.ti.com/power-designer/switching-regulator/customize/12?noparams=0

    Let me know if you have further questions

    Thanks,

    Prateek