Part Number: ISOM8600
Hi,
One of my application, i planned to use the IC. I just want to know the maximum & min switching frequency and max operating voltage between S1 & S2.
Regards,
Vignesh M
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ISOM8600
Hi,
One of my application, i planned to use the IC. I just want to know the maximum & min switching frequency and max operating voltage between S1 & S2.
Regards,
Vignesh M
Hello Vignesh,
Thank you for reaching out. As you have noticed, the ISOM8600 is used for switching burden resistors and other inputs. It's switching performance is not tied to a specific interface standard for isolated switching. Therefore, the maximum and minimum switching frequency is not strictly defined.
The below switching characteristics table can be used to provide a maximum switching frequency using F_max = 1/(TON+TOFF) = 2.5kHz. This calculation only includes the ON and OFF response time, and I would recommend adding the amount of time your application needs an ON and OFF asserted. Adding these hold times will create a healthy margin that is more appropriate for your applications.

Best,
Andrew