Part Number: ISO7720-Q1
In my design, I plan on using ISO772x or ISO642x devices for translating data across high voltage, while running a wideband low-noise ultrasound amplifier in proximity on the same PCB. I was concerned about what the keying frequency for the carrier was, considering my amplifier bandwidth extends to 1GHz, and if radiated emissions would be significantly present on the output signal given 50+dB of gain. I was also curious what the EMI reduction techniques of these devices consisted of, and if the modulation oscillator is free-running or only active while data is being passed. Do either of these device series have lower radiated emissions than the other?
If these parts would not be suitable considering the requirements, would there be an alternative part you would recommend?