Part Number: ISO7721
Hello,
we have some trobules with overvoltage situations on pins OUTA and INB. In our case we use a 3.3V protection diode on these pins, but in some situations we have device failures. In this case VCC1 and GND1 get shorted in the ISO7721.
To do some further protection I need to know the maximum allowed current injected on OUTA and INB for e.g. 500ms.
My idea, current runs into device, through protection diode to VCCI. VCCI gets a shunt referece to limit the voltage to e.g. 4.7V.
Thanks!
Regards Konrad