Part Number: ISO7041-Q1
Other Parts Discussed in Thread: ISO7041
Hi,
We are currently using the ISO7041-Q1 as an interface between the microcontroller and the UIR IC for SPI communication. As per the datasheet recommendation, we have implemented 300R ohm series resistors on both the input and output sides of the isolator.
However, we are observing that SPI communication gets interrupted when these series resistors are in place. When the resistors on the MOSI and CLK lines are replaced with 0R ohm (shorted), the SPI communication is restored and operates as expected.
We would like to understand the possible reasons for this behavior. Specifically:
- Could the series resistance be impacting signal integrity (rise/fall times or edge distortion) at our operating SPI frequency?
- Are there recommended resistor values or design guidelines for SPI lines when using this isolator?
- Should the resistor values be adjusted based on trace length, load capacitance, or SPI clock speed?
It would be helpful if you could provide guidance on selecting appropriate series resistor values for reliable SPI communication with this isolator.