Part Number: ISOW1432
Hi Team,
part Number: ISOW1432DFMR
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ISOW1432
Hi Team,
part Number: ISOW1432DFMR
Hi Venkata,
Thanks for reaching out. Please find my inputs below:
The IN and OUT pins on the ISOW1432DFMR form a dedicated 2 Mbps unidirectional GPIO channel that transmits digital signals across the galvanic isolation barrier, independent of the RS-485 transceiver. This channel eliminates the need for a separate digital isolator or optocoupler for auxiliary signals [1][2].
The signal flows from IN → across the SiO₂ capacitive isolation barrier → OUT
Note: "IN" here stands for the GPIO input pin, not "Intelligent Network."
The GPIO channel is designed for transmitting diagnostic or status signals from the bus side back to the MCU, such as:
|
Pin
|
If Unused
|
|---|---|
|
IN
|
Tie to GND (default LOW state) to minimize power consumption and noise coupling
|
|
OUT
|
Can be left floating — outputs don't pick up noise
|
The IN/OUT GPIO channel provides a simple, isolated digital path for auxiliary signals, letting you monitor bus-side power status or transmit control signals to the MCU without adding discrete isolation components to your design.
You can also refer "Applications" section in this app brief for example use case of GPIO pin - Optimize Your Design with Isolated RS-485 Transceivers with Integrated Power
Regards
Varun