Part Number: ISO6441
In ISO7241, there was an issue where noise was introduced when a 1 GHz impulse response(pulse) was applied. Since this is believed to be caused by the edge-based architecture, I assume that ISO 7741/ISO 6441 improves noise immunity by adopting the OOK method and does not allow the 1 GHz impulse response to pass through. Is there any actual test data or documentation regarding the impulse response?