Part Number: ISO7761
Hi everyone,
i found the description of the creepage definition:
The shortest path between two conductive parts measured along the surface of the insulation.
A common practice is to add grooves in the PCB to increase the creepage distance. Is this correct, because the IC is directly above the PCB and no distance between the bottom side of the IC and (!) the PCB itself. I have the fear, that during certification the lab can complaint in the way that the bottom side of the IC "shorten" a possible creepage groove.
Does anyone got feedback during certification during usage of grooves?
Best regards