Part Number: ISO6521
ISO6521 datasheet shows (chapter 7.4.1) that there are inner diodes on each input (also specified in absolute maximum ratings, the "+/-0.5V"). In my application there may be occasional (=surge/exception) situations where input voltage can go beyond local supply. I intend to add series resistors with inputs for such situations. To properly size these resistors, I need to know the absolute maximum value for the input current, when the inner diodes are conducting.