Part Number: ISO7763-Q1
Is there a spec for the maximum current the input diode structures can handle? Seeing some parts fail despite having sizeable series resistance on the inputs. During shutdown for a 100ms or so the input on the secondary side is around 0.5V while the power rail is off, but the current into the pin is in 70-150uA range at most. Despite that the pin ends up shorted to ground.
Secondly, is there way to get a quick design review to rule out any possible issues causing this?