Part Number: ISO1228
I have followed the reference design in the ISO1228 datasheet for source/sink mode with the back-to-back LEDs for each channel on the LEDx pins. What I have found, is that in sink mode, the LEDs work properly. However, in source mode, the LEDs are quite bright even when the inputs are disconnected. They do get brighter when an input is active, but why are they on at all? Does the chip have high internal leakage, or could this be the wire break detection current? The LEDs I am using are APHB1608LVBDZGKC. Thanks