Part Number: ISOM8610
Our design uses a competitor part which is tested, analysed and working but going obsolete. A potential replacement is ISOM8610. It is the only suitable replacement that appears available on the market due to various specification requirements. Functionally, the device behaviour is completely appropriate but the isolation may be a problem and the datasheet is unclear.
For our requirement, we must be able to test isolation withstand for 1400Vdc (or 1000Vrms) for 60s on each production item. This would be seen across the ISOM8610. I have read 8.2.4 in the datasheet and I need to be certain - is the graph implying that the device will withstand >7000Vrms when tested for 60s? And that the 500Vrms or 707Vpk is only if we need the voltage applied over a period of 20/30 years?
Thank you.