This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO1050



  1. In the datasheet it specifies VCC2 the recommended operating conditions  to be  4.75V to 5.25V, what would/could happen if VCC2 is operated at 3.3V?

  2. In the Undervoltage Lockout and Fail Safe section if VCC2 falls below 2.7V the transceiver will lock out.  What is the hysteresis for this function and the range for this function?  We are seeing it drop out 3.24V

  3. After an undervoltage lock out does the controlling DSP need to perform a TXD sequence to get the transceiver to start back up or is it automatic?

  4. Is there a mode or condition that will let the transceiver transmit but not receive?

 

Thank you for your help with my questions.

 

Regards