Hi Community,
I'm relatively new to serial communication, RS485 in particular and I hope you can help me understanding the ISO3086.
The scenario:
Two devices are talking to each other over a long (but variable) distance. Since it is a rough environment and the cable length inbetween the two devices can vary from 50m up to 500m, I decided to use RS422 communication and also decided to use an isolated interface.
First question:
The datasheet of the 3086 says, it has an internal fail-safe bias network.
Does that mean, I do not have to add bias resistors to pull the A/B lines to a defined state when the cable is disconnected?
If so, I still need to add the 120 Ohm resistor inbetween A and B, right?
Second question:
The cable that is being used does only have two wires. Thus, I cannot have a separate GND wire inbetween the two transceivers.
So what do I do with the VCC2 and GND2 on the isolated side of tranceivers? Can I put a DC/DC converter to have an isolated power supply and connect that to VCC2/GND2? Or do I just connect VCC2 to the isolated Power Supply and leave GND2 open?
I have attached the schematics of how I would put the 120 Ohm resistors... is that correct?
Any help or hint is highly appreciated as I have never really used this component before nor have a used rs422 in the past.
Thanks a lot in advance,