The component ISO1050DW is it compliant with the IEC 60601-1 ed3 A1? I don't find its certification.
Thanks in advance.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The component ISO1050DW is it compliant with the IEC 60601-1 ed3 A1? I don't find its certification.
Thanks in advance.
ISO1050DW is certified according to IEC 60601-1 Ed 3 up 125 Vrms 2 MOPP. Please see CSA certificate starting page 32 of the link below:

I'm checking with the certification agency if amendment 1 will require additional testing at component level? and whether those requirements can be handled at system-level?
I expect to hear back next week as my agency contact is out of office this week.
I just heard back from CSA. This device still meets the requirements of IEC 60601-1 3rd Ed Amendment 1 because the provisions in amendment 1 don't impact these components.