Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Is the iso7420 appropiate for this aplication

Other Parts Discussed in Thread: TPS28226, ISO7420, ISO7820, ISO7320C, ISO7720, ISO7740

Hi!
I want to generate pwm signal for the mosfet's gate of a buck converter, and i'm generating the pwm signal from a fpga. I need to protect my fpga, so i'm going to use iso7420 isolator and that signal is going to tps28226. Finally, the signal from the tps28226 go to the gate of mosfet.


I need a 1 MHz frequency for my pwm signal, but i don't know if the iso724 is appropriate for this aplication.

Is the iso724 idel for this system?