Other Parts Discussed in Thread: ISO1540
Hi,
In ISO1540 datasheet, the absolute maximum rating for SDA2 pin is defined as "VCC2 + 0.5V" with a note "Maximum voltage must not exceed 6 V."
Considering VCC2 is 3.3V, what is the absolute maximum rating for SDA2? Is it 3.8V or 6V?
Thanks!
Antony