Hi~
In ISO7231 datasheet, it suggest to use 4 layer PCB for proper communication, but customer want to use 1 layer PCB.
Is there any guideline or special point for 1 layer isolator design?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi~
In ISO7231 datasheet, it suggest to use 4 layer PCB for proper communication, but customer want to use 1 layer PCB.
Is there any guideline or special point for 1 layer isolator design?
Thanks.
Hi Jin-Suk,
We have not done any testing on ISO723x with a 1 layer PCB. I think this maybe ok for low data-rates (<10Mbps) but may be difficult for higher data-rates. I would suggest including 100 Ohm resistors in the path of the output buffers to slow down the rise/fall times. Similarly, the devices driving the ISO723x should have slow rise fall times. Also place the bypass capacitor on VCC1 and VCC2, between pins 1 and 2, and between pins 15 and 16 respectively.
Regarding the reflow temperature, upto 260 C is supported.
This is described in the Addendum-Page 1 under MSL Peak Temp: "Level-3-260C-168 HR"
Rgds,
Anant