Other Parts Discussed in Thread: ISO5852SEVM, ISO5852S, TIDA-00195
Hi,
I have a task to develop a multi-channel power controller. It have to control temperature in the IR oven. The source of the control signal is a controller and the driver - ISO5852, a control signal for the driver - PWM 1 kHz. The driver will drive a powerful IGBT transistor. I assembled a prototype according to the scheme ISO5852SEVM. As the power supply, I installed a diode bridge on the line 230V AC. To supply driver 16 VDC unipolar power supply has been used.
When I used as a load 230V 100W incandescent lamp it works fine with IGBT and MOSFET transistors. When I increased the load, using the IR lamp 1000W 230V, ISO5852 protected MOSFET transistor during the cold start lamp when passing a very high current. Then I set the IGBT transistor instead MOSFET and the driver was not defend the transistor.
A cold start lamp is similar to the short-circuit mode, but the driver still had to protect the transistor. MOSFET transistor I used IRFP350, IGBT - STGW40M120DF3.
Please tell me where I made a mistake. Why the driver does not protect the IGBT transistor?
Is there any solution, how can we solve the cold start problem for infrared lamps?