Other Parts Discussed in Thread: ISO1050
Hi Iso team,
I have a customer who wants to isolate his CAN bus, but they don't like the fact that the ISO1050 takes the CAN_L and CAN_H signals and converts them to TX and RX digital lines (so iso + transceiver in one). They would prefer the part take CAN_L and CAN_H signals in, and have CAN_L and CAN_H signals out.
Can we use a different digital isolator (without the integrated transciever) to achieve this? the problem i see there is the CAN_L and CAN_H lines essentially reference different high and low levels, so it almost sounds like we would need two digital isolators, one with an input VCC of 3.5V and GND of 2.5V, and another with an input VCC of 2.5V and GND of 1.5V....
There's the 1MBPS datarate to factor in as well.
Any ideas on the best way to achieve this and/or part recommendations?