Hi,
I'm building a three-phase IGBT inverter, and I'm looking at options for the gate drivers. I'm using 1.2kV IGBTs, and this is a flexible prototype so I'd like the drivers to have a high peak current capability.
The ISO5452 looks almost ideal as it has most of the features I'd like (active Miller clamp, overcurrent (desat) fault detection, UVLO, split outputs for control over turn-on/off currents, fault alarm and reset). The only problem is that this is a single-channel device.
The best dual-channel gate driver I can find is the UCC21520. It has a peak 4A/6A source/sink current output, programmable deadtime, and a disable pin. The problem with this device is it's missing the active safety features (and less important for me, the split outputs) of it's single-channel counterpart, the ISO5452.
Just wondering if there's a product or solution to combine the active safety features of the the single-channel device, with the deadtime provided by the dual-channel device? There seem t be plenty of dual-channel drivers for MOSFETs, but I can't find any for IGBTs that incorporate features like Miller clamp and desat detection. Should I just rely on the microcontroller code to never turn both IGBTs on?
Thanks!