Hi everyone,
I am using the ISO3082 as Dual Isolated Half-Duplex RS485/TTL conversor. I am following the Reference Desing TIDU590, but on the TTL side I have a microcontroller which receives R, and D in a UART and D and /RE are controlled with a GPIO as Digital output (8mA) .
I have tested this configuration: MCU with the SN65HV82 (RS845/TTL conversor but not isolated) without problems however I am having problems with the Isolated one.
I can receive properly from RS485 to the microcontroller (I check in the oscilloscope A and B signals, perfectly inverted). But from MCU to RS485, something is not working: I can check the answer signal (D) from the MCU to the ISO3082, also the control signal (D/RE). But at the output of the ISO3082, A and B signals followed D but they are not inverted so it is not recognized as RS485.
Any idea of what could it be happening?
Thanks in advance
Best regards