Hi, we are using 2 PCA9518 I2C expanders to create a 1 to 4 I2C expander. That circuit is working good, but now we have to isolate the I2C interface and want to use the ISO1540 in front of the PCA9518 which runs at 3.3V. Will those 2 parts play nice together? I'm concerned as the PCA9518 creates a 0.5V ledge on the SDA bus and not sure if that will interfere with the ISO1540 direction detection. The side 2 spec of the ISO1540 says 0.3 x VCC2 (0.99v) for Vil2, so it appears that it would meet that spec, but not sure......
Thanks - Robb