Hi,
I am using I2C to communicate with a remote sensor. I want to turn the 3.3V to the sensor off between readings. If I use a ISO1541 for isolation of the I2C bus I would have 3.3V on VDD1 and 0V on VDD2 in the "off" state. The datasheet says that would put the device in "lockout". I have three questions:
1.) Is this a valid way to try to use the device?
2.) How much current is the device going to draw when Vdd1 is 3.3V and Vdd2 is 0V
3.) When VDD2 comes up to 3.3V is the device going to work or could it latch up?
Thanks,
Greg