This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7740: SSOP version

Guru 20090 points

Part Number: ISO7740

Hello,

Are there any road map for SSOP package of ISO7740?
Our customer request the Low I/O voltage (under 2.5V) and small package (SSOP) device.
Since the FPGA IO voltage is decreased, they may not use 3.3V , 2.8V IO from now on.

Best Regards,
Ryuji Asaka