Part Number: ISOW7841
Other Parts Discussed in Thread: SN65HVD72, SN65HVD1473, TIDA-00892
Hi,
I plan to evaluate it by connecting SN65HVD72 and ISOW7841.
(Operate at 3.3V-3.3V, 0.25MHz)
Is it possible to operate the SN65HVD72 with the isolated power supply Viso of the ISOW7841?
From the datasheet of ISOW7841, Iiso(out)=74mA,
datasheet of SN65HVD72 from Figure6 I think that Icc needs about 62mA.
I think that the isolation current of the power supply side (ISOW7841) is 74mA and
the SN65HVD72 of the target is 62mA, so I think that there is no problem with current capacity,
but can it be used without problems? Is it?
※I think that the consumption current of the insulation side power supply is expressed by Iiso(out), but is this output current?
In the case of output current, is the current value of the insulation side power supply written in the data sheet? Please tell me.
best regards