Part Number: ISO1050
Hello Team,
My customer uses our ISO1050, their application is as below, there are 14 CAN loads(2 MPU and 12 PM) on the BUS. And the schematic for each load is as below. Customer test the CANH and CANL on MPUB. They find when they insert any PM board, tthere are abnormal waveforms of CANH and CANL, the frequency is about 38kHz, after short time, the CANH and CANL waveforms are ok. You can find the waveform below. Can you help to explain why there are some abnormal waveform when insert any PM board? Thanks
Regards,
Nanfang