This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO1212: Application note

Part Number: ISO1212


Dear Sir 

I saw ISO1212 application note have below figure

May I know Why the traditional solution have 84.1°C ? What's component cause this temperature ??

The competing solution is ISO1I811T ?

  • Hi Kai,

    The traditional solution uses a basic current limit, which can draw close to 12mA current for 32V input. For eight channels this results in a power loss of 3W. This excessive power dissipation causes the board temperature to rise.

    Can you please contact me at anantkamath@ti.com? I can provide more details of our test setup, and the competition device used.

    Rgds,

    Anant