Part Number: ISO1211
Other Parts Discussed in Thread: DRV8803, TPS27S100
Hi Sirs,
We're survey digital isolators solution.
Could you check ISO1211 is suitable solution?
If not, have others solution can share?
Thanks!!
My spec requirement as below
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Shu-Cheng LIN,
ISO1211 can be configured to meet "Isolated Digital GPIO Input Usage" requirements by adjusting the external Rthr and Rsense resistor value as mentioned in data sheet. Except for the off-state voltage (LOW): 0 to +4V parameter, please let me know how stringent is this parameter? (for more details on current and threshold voltage configuration, please refer "Electrical characteristics—DC Specification" section of the datasheet.).
And as ISO1211 is a receiver device, it cannot be used for "Isolated Digital GPIO Output Usage". I don't think we have any Isolated device that can be directly used for output usage.
To understand the system better and to provide application specific suggestions, Can you please share more details about the end equipment and application?
Thanks.
Regards
Tejas
Hi Shu-Cheng LIN,
Yes, ISO1211 can meet digital input requirement.
For Digital output, we have a design suggestion that can be used. Can you please share your email id and we will get in touch with you.
Thanks.
Regards
Tejas
Hi Sirs,
Thanks!
Please help send mail to
Billy_Lin@pegatroncorp.com, jchen@ti.com and eric.sc-lin@wtmec.com
Hi Sirs,
We did not receive the e-mail . Could you please also check if TPS4H160 is a suitable solution to meet our digital out requirements.
If yes, What the difference between DRV8803 and TPS4H160?
Thank you.
Hi Shu-Cheng,
Sorry for delay in response, I have started a email thread, lets continue the discussion over email.
Thanks,
Regards
Tejas