This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISOW7841: Capacitance of the Isolation Transformer windings

Part Number: ISOW7841


Hello all,

Is it possible for you to provide the capacitance of the Isolation Transformer windings?

Reference datasheet page 1 Simplified Schematic.
 

  • Hi Daniel,

    I am assuming you are asking the capacitance formed between side 1 and side 2.
    We do measure the capacitance between side1 and side2 by shorting all the pins on the respective side together. This value is ~3.5pF.
    Please refer to section 7.6 of datasheet for additional details about the "CIO" parameter.

    Let me know if this answers your question or if additional details are required.
    Thanks.

    Regards,
    Anand Reghunathan