Part Number: ISOW7841
I want to useISOW7841 digital isolator in my project .But i want to know that will it make any radiation effects in the board??.
This isolator is used in one daughter board ,which is used to measure both current and voltages. This board is having 32 isolated channels,processors and power supplies,etc. The board dimension is 125mm * 85mm. the components are almost tightly packed on the top and bottom layers. The isolators will be on both layers. The daughter board will be plugged in the main board ,both boards will have 10mm gap.Both board will communicates through FMC-HPC Connector.
Is it make any radiation problems in the board itself or in the main boar?
what are precautions should I take to avoid the radiated emission ?
Please help me to get the best design