Part Number: ISOW7841
Hi Team,
Is there are way to decrease ISOW7841's EMI level in 200~240MHz range? Or is there are way to 200~240Mhz EMI level to higher frequency range? Like dithering function, etc...
One of my customer is using ISOW7841 and got have problem with EMI test result
The customer fail to pass the EMI test in 200~240Mhz range
Overall, customer's the EMI test result waveform is so similar with TI's test result (Figure 3 in http://www.ti.com/lit/an/slla368a/slla368a.pdf ) and high EMI value in below red-circle area and it overs boundry
Customer try to decrease the EMI level in 200~240Mhz(Adding CAP, layout, etc), but still have problem and inquired to TI to ask whether there are way to decrease the EMI in specific frequency range or switch the EMI peak level frequency
Please let me have your answer
Thank you