Part Number: ISO7742
Other Parts Discussed in Thread: ISO7741
Dears:
Could you kindly help to check whether the solution is OK as below:
ISO7742 is powered with different values: VCC1 is 3.3V, and VCC2 is 5V.
Since we are replacing the ADI's PN(ADUM1412), and ADI support the function.
From our datasheet I can see ISO774X support 2.25-V to 5.5-V Level Translation, however, there is no Supply Current Characteristics about the customer's application.
Could you kindly help to check it?
Thanks a lot!
Best regards
Luck Wu