Part Number: ISOW7841
Hello,
currently I am working on a design in which ISOW7841 is used to isolate two areas of the PCB. 3.3V are used at both sides.
I have seen on the application notes and some reference designs that configuration 1 (see image below) is preferred.
Is there any real issue using configuration 2 or configuration 3? If so, what is it?
In case there is no real issue using configuration 2, what is the minimum width of the narrow no-copper part? I guess it is related to the maximum voltage isolation that you want. The design will be powered by 5V USB connected to a PC and is part of a medical device.
Thanks in advance,
Alejandro