Part Number: ISO7710
Dear Team,
our customer would like to use the ISO7710 in an input module. The front end is powered from the input, meaning that is turning on and off. The output / the other side @ VCC2 is constantly on.
I saw in the referred post, that the output could be giving some pulses during the start-up because the default out is HIGH. So as per my understanding, it might be better to use the F version to have LOW in those situations.
Could you please confirm that this is not a problem?
Is there any risk of having spurious glitches or any starting oscillation if VCC1 is ramping slow?
Do you also have more information about the start-up time? I saw in another post that the max. start-up time is 180us. Do we have a typical value for this?
Thanks and best regards
Martin