Part Number: ISO7742
Hi,
according 8.4.1,
Could you provide the maximum average forward rectified current for the ESD Diode ?
(Please refer to the picture as below, marked with red frame.)
Thanks,
Regards,
Ben
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ISO7742
Hi,
according 8.4.1,
Could you provide the maximum average forward rectified current for the ESD Diode ?
(Please refer to the picture as below, marked with red frame.)
Thanks,
Regards,
Ben
Hi Ben,
Thank you for using E2E. The ESD diodes given in Figure 8.4.1 are primarily meant for ESD protection & clamping, it is not recommended to pass continuous current through these diodes. Applying INx higher than its respective VCC violates the absolute maximum rating of INx pin as shown below hence passing continuous current through ESD diodes will violate device absolute max specs.
These ESD diodes are designed to meet 6kV HBM ESD.
Regards,
Koteshwar Rao