This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7761: Connections for unused channels

Part Number: ISO7761


Hi,

How should be the connection if any of the channel for ISO7761 is not used? 

Connected to GND, pull up or NC? both at the input and output of the related channel?

Best Regards,

Caglar

  • Hi Caglar,

    For the input pins of unused channels, leaving them floating is not an issue but we recommend them to be connected to their default state to avoid any noise pick-up. e.g., for device ISO7761 (default HIGH, without suffix 'F') it is recommended to connect input pin to VCC through a pull-up resistor (typically 4.7kΩ). For ISO7761F (default LOW), it is recommended to connect the input pin to GND.

    For the output pins of unused channels, it is best if they are left floating. Let me know if you have any questions on this, thanks.


    Regards,
    Koteshwar Rao