This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7760: ISO7760 succeed cases

Part Number: ISO7760


can you give some ISO7760 succeed cases

  • Hi,

    We have many 3-phase Servo Motor Drive customers using ISO7760 for isolating the IPM modules. The device is also largely used in Factory Automation where there is a high density of input/output channels. Since the digital isolator family ISO77xx meets isolation requirements for many application, the device is being used in various other applications as well.

    Could you please describe what application are you looking to use ISO7760 for? Are there any questions or concerns you would like us to clarify you? Thanks.


    Regards,
    Koteshwar Rao