This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am trying to drive a n-mosfet (30n60 IC) with ISO5500EVM. The issue is, I am not getting the control signal given to input put PIN (TP4) in the left side at output side .(Vout in the right side)
My connections are
left side
5 Volt between TP10 and TP9
control signal to TP4
TP3 and TP4 are connected to the ground
right side
S, D, and G points are connected to source , drain and gate of the mosfet. And a load is connected to the mosfet and 20 volts is given between the mosfet and the load.
15 Volt is given between TP12 and TP11
It would be really helpful if you could let me know the correct connections.
Hi Siddiq,
It may due to incorrect connection on the DESAT pin. Could you please try to connect JMP2 to see if you can get an output?
Also could you draw a schematic of the MOSFET connection to the external 20V supply?
With Regards,
Xiong