Part Number: ISO3086
Hi Sir
May I know how to increase VOD magnitude when RL= 60ohm
I saw ADI solution can be reach to VOD maximum value,but TI doesn't have maximum value
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kai,
Thank you for using our E2E forums!
For a given part, there are a few ways to increase Vod:
However in this case, the resistor is fixed at 60 ohms, so the easiest way in this case is the first option. The allowed range for Vcc2 is 4.5 to 5.5V. So the customer can use the higher end of Vcc2 to improve this. Is there a target value needed? The 3086 easily provides the 1.5V minimum required for bus communications.
The maximum value is limited internally to the value of Vcc2 rail. [best case]. Please see screenshot below from the datasheet:
Hope this helps.
Regards,
abhi