Part Number: ISO7760
Hello,
We are using ISO7760 for isolating PWM signals provided to a multiple gate drivers. However, we are now noticing that the output of ISO7760 is being pulled down periodically. Please find the attached cases.
1. A high signal is given at the input but the output isn't continuously high.
2. A fixed duty 25khz signal is given at the input. However the output is pulled down for certain amount periodically.
Please suggest what could be the possible issue.
Regards,
Shyama
1. High In
The output PWM Duty and Frequency is correct. It is just that output is pulled down periodically as seen above.