This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7641FC: Equation of the average lifetime

Part Number: ISO7641FC


Hi,


Could you show me equation of the average lifetime?
They seem to want to know how to calculate lifetime.

This question is related to below thread.

Best Regards,

Kuramochi

  • Hi Kuramochi-san,

    We do not have any equation for the average lifetime of ISO7641FC. The lifetime plot that we provide is generating from the lifetime test called Time Dependent Dielectric Breakdown (TDDB) which is a standard test practiced in the industry to find out device's lifetime.

    The basic test methodology is to apply a stress voltage from the input to the output of the DUT in a two-terminal configuration using a high-voltage source, while maintaining the still-air, ambient-air temperature at 150°C. The start of the test activates a timer; this timer is stopped when the current in the circuit exceeds a particular fail current level (like 100uA), which meant that the dielectric had failed. The time taken by device is noted for each applied test voltage. DUTs were tested independently of each other (one DUT per test) at each test voltage to get statistically valid results. Sufficient number of devices are tested at multiple test voltages to get the most practical device lifetime curve.

    I hope this answers your question, thank you.


    Regards,
    Koteshwar Rao
  • Rao-san,

    Thank you for your quick response.
    Could you provide the lifetime plot?
    My customer would like to get the reason of lifetime value.

    Best Regards,
    Kuramochi
  • Hi Kuramochi-san,

    I noticed that you have made your e-mail ID available to everybody in the E2E community. I will write you a separate email to you regarding your request for the TDDB data. Thanks.


    Regards,
    Koteshwar Rao