This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7740: ON/OFF Control

Part Number: ISO7740
Other Parts Discussed in Thread: ISO7710

Hi, Team,

My customer want to improve the life time for the OPTO, they want to choose the digital Isolator. Can ISO7740 support the ON/OFF control(Such as the input signal always high in the ON condition)? Do you have other low cost solution for this? Thanks!

  • Hi Wu,

    Yes, TI digital isolators like ISO7740 can be used to replace opto couplers and input can be static ON/OFF or can be dynamic data with datarate upto 100Mbps.

    ISO7740 is a 4 channel device that replaces 4 opto couplers. If you are only looking for one channel then you can use ISO7710 that will be lower cost than ISO7740. Thanks.


    Regards,
    Koteshwar Rao