Hi
in SN6505B datasheet, the Absolute Maximum Ratings Peak output switch current @ 25 degree C is 2.4A.
Recommended Operating Conditions Output switch current - Primary side is 1A.
now customer's application input is 5V, they can see 1.2A peak inrush current at SN6505B startup, and in some projects, the output capacitor is even larger, so the peak current will be 1.8A. inrush current waveform is as below.
customer want to know what's the Absolute Maximum Ratings Peak output switch current @ 90 degree C of SN6505B?
can 1.8A inrush current be support by SN6505B at 90 degree C?