Part Number: ISO7820LL
Hi,
I use ISO7820LL to transmit LVDS signal. But i met a question on GND.
Please refer below schematic,
If 3(the VCC1 GND of ISO7820LL) is connection for VCC1, OUTA+ and OUTA-(FP_SYNC_P, FP_SYNC_N) is no output.
If 3(the VCC1 GND of ISO7820LL) is connection for the reference ground of 1 and 2 (INPUT LVDS signal), the output of OUTA+ and OUTA-(FP_SYNC_P, FP_SYNC_N) is OK.
The GND1 should be connection for VCC1 shown in datasheet, but why fail in the actual test.
Thanks,
Walsh