Part Number: ISO1212
Other Parts Discussed in Thread: , ISO1211
Customer would like to design the ISO1212 for AC motor. There are some questions related to the ISO1212's performance and design.
1. How to calculate the power consumption of the chip?
2. How to select the C3 filter value on ISO1212EVM with consideration of the minimux turn-on duty ?
3. What's the abxMAX current through into Pin7 of the device?
4. How much the current going though to pin 8 of the device?
5. Is Turn-ON threshold able to be adjusted to 3V, and Turn-Off be ajusted to 2V?