Other Parts Discussed in Thread: ISO7840
Hi, a customer is working on a project wihere Viowm 1000VDC(707VAC) with EN61010 reinforced is needed.
ISO7762:
ISO7840:
At the two digital isolators the datasheet refers to EN61010.
Eg. ISO7840:
5700Vrms REINFORCED insulation per EN 61010-1:2010(3rd Ed)
up to working voltage of 600Vrms(DW package) and 1000Vrms (DWW package).
Does the reinforced only refers to the insulation of 5700Vrms or is the information for the operating voltage as well reinforced, which then would relate to BASIC of operating voltage of 2000Vrms.
A concrete statement is needed here, because in case of REINFORCED the 1000Vrms/1414Vdc would be sufficient.
In case of BASIC, the 1000V/2 = 500Vrms/707Vdc would be too low.
Thank you!
Fred