Part Number: ISO1540
I use ISO1540 (see original discussion on
), but the data is wrong after the isolation
This is from the slave side, and the signal looks good (there is a tiny step near the right side of the screen, but it will not be mistaken as logic 1)
This is from the master side, and the tiny step is now a big step there, over 0.8V, and the 3.3V micro can easily read it as 1
Any pointer for resolve this?
Thanks!