Other Parts Discussed in Thread: TIDA-00893
Hi Sir,
Our customer used the ISOW7841, But EMI report Fail.
Could you please support for Review Layout?
or based on EMI report Could you please provide the suggest for me?
Hugo
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sir,
Our customer used the ISOW7841, But EMI report Fail.
Could you please support for Review Layout?
or based on EMI report Could you please provide the suggest for me?
Hugo
Hi Hugo,
ISOW7841 emissions are affected by factors such as layout and operating conditions. Can you include more detail of the setup? For example, what are the Vcc and Viso values? What is the load on Viso?
PCB layout can greatly improve performance if designed using the considerations in this application report. Please encourage our customer to review their board layout to ensure it includes a stitching capacitor and y-capacitor as mentioned in the linked app report. Additional comments regarding common mode chokes are provided in this E2E post.
Is this helpful? Please let me know!
Thank you for posting on E2E,
Manuel Chavez
Hi Sir,
Thank for your explanation.
our customer tell me , VISO load <20mA(5V),
But for test COM port only have cable, the device not power on EMI is over spec.
The USB/LAN/RS232/DP connector is on same PCB, if note "EUT only" is not connect to any deice(USB/LAN/RS232/DP).
They are try to COM port metal case to GND, EMI 400~500MHz base will be reduce.
They are doubt this issue is fromCOM port ground.
we have some question, could you please share your suggest for me?
Q1, we are see the TIDA-00893 & slla368b have different equation for Ci. we can ref which one?
Q2, we are try to calculate Ci Value as below, need change to >50pF? I see the D(mm) only 0.1 any risk?
Q3, the slla368b Figure 5(RF+L1) & Figure13(Common-Mode Chokes) to reduce emissions, Is this only one on PCB or both use?
Hugo
| K=Er(4.2 for FR4) | Eo(F/m) | D(mm) | L(mm) | W(mm) | C(pf) | ||
| PCB | 4.2 | 8.854E-12 | 0.6 | 77.3 | 6.28 | 3.00868E-11 | TI ref design |
| PCB | 4.2 | 8.854E-12 | 0.1 | 30.8 | 2.62 | 3.00083E-11 | Customer COM1 |
| PCB | 4.2 | 8.854E-12 | 0.1 | 20.16 | 4.01 | 3.00624E-11 | Customer COM2 |